Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description

Full-filled Configuration (Downlink)

Bandwidth

Choices:

Downlink: Based on the Table 5.3.2-1 and 5.3.2-2 in 38.104

Uplink: Based on the Table 5.3.2-1 in 38.101-1 and 38.101-2

Selects the bandwidth configuration for the carrier.

Numerology

Selects the numerology of the configuration. The choices are related to the selected bandwidth.

Duplex Type

Choices: TDD | FDD

Selects the duplex type.

When TDD is selected, several TDD parameters appear below. These TDD parameters are reset to default values whenever numerology changes or FR changes. (The default values are different for each numerology.)

Transmission Periodicity

Sets the periodicity of DL-UL pattern. The choices are related to numerology.

Number of Downlink Slots

Sets the number of consecutive full DL slots at the beginning of each DL-UL pattern. The range is related to the numerology and slot configuration period.

Number of Downlink Symbols

Range: 0 ~ 14 for Normal CP; 0 ~ 12 for Extended CP

Sets the number of consecutive DL symbols in the beginning of the slot following the last full DL slot.

Number of Uplink Slots

Sets the number of consecutive full UL slots at the end of each DL-UL pattern. The range is related to the numerology and slot configuration period.

Number of Uplink Symbols

Range: 0 ~ 14 for Normal CP; 0 ~ 12 for Extended CP

Sets the number of consecutive UL symbols in the end of the slot preceding the first full UL slot.

Number of Special Slots

Displays the number of special slots.

TDD Slot Allocation

Displays the TDD slot allocation for one period.

Modulation

Choices: pi/2 BPSK | QPSK | 16QAM | 64QAM | 256QAM for uplink carrier; QPSK | 16QAM | 64QAM | 256QAM for downlink carrier

Select the Modulation type to be configured for current carrier.